Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / DataCriteria Class / IntervalMicroseconds Field


In This Topic
    IntervalMicroseconds Field
    In This Topic
    Establish a number of milliseconds between data samples for a query.
    Syntax
    Public IntervalMicroseconds As System.Long
    public System.long IntervalMicroseconds
    public:
    System.int64 IntervalMicroseconds
    Requirements

    Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

    See Also