Managing Historian Systems
Access a System
Procedure
Add a System
Before you begin
About this task
If you want to manage a Historian system using Configuration Hub, you must add it to Configuration Hub.
Procedure
What to do next
- As needed, add another data store.
- If you want to create a horizontally scalable system, the machine that you have added serves as the primary server. On the machines that you want to use as distributed servers, you must install Historian distributed nodes and then add them to the system.
Add a Distributed/Mirror Machine
Before you begin
- Install Historian distributed server on the machine that you want to add as a distributed server.
- Add a system. The server that you specify while adding the system serves as the primary server for the system.
About this task
Procedure
What to do next
Remove a Distributed Machine
Before you begin
- Delete the data stores in the machine (using the Web Admin console).
- If the machine is added to a mirror location, remove it from the location.
Procedure
Set a Default Location
About this task
- You can have only one default location in a system.
- You cannot delete a default location.
- You can set any of the distributed or mirror locations as default.
Procedure
Create a Mirror Location
Before you begin
About this task
If you want high availability of one or more data stores, you must create a mirror group (also called a mirror location), and then add servers to it. When you do so, the data in the data stores of the mirror locations is replicated. Therefore, even if one of the servers is down, you can retrieve data from the other servers in the mirror location, thus achieving high availability.
- You must add minimum two servers to a mirror location. The maximum number of servers that you can add depends on your Historian license.
- You can add a mirror location only in a horizontally scalable Historian system.
- You can rename a mirror location, remove a machine from a mirror location, or add an additional one even after you create the mirror location. However, if only one machine remains in the group, you cannot remove it.
Procedure
What to do next
Rename a Mirror Location
Procedure
Add a Machine to a Mirror Location
Before you begin
- Copy the archive files and configuration files from an existing machine in the mirror location to the one that you have added.
- Rename the configuration file <machine name>_Config.ihc.
Procedure
Remove a Machine from a Mirror Location
About this task
Procedure
Delete a Mirror Location
Before you begin
Procedure
Modify a Historian System
About this task
- Name
- Description
Procedure
Set a Default System
About this task
- You can have only one default system in Configuration Hub.
- You cannot delete a default system.