Work with Data Stores
Configure Data Stores
A data store is logical collection of tags used to store, organize, and manage tags according to the data source and storage requirements. A data store can have multiple archive files (*.IHA), and includes both logical and physical storage definitions.
Tags can be segregated into separate archives through the use of data stores. The primary use of data stores is to segregate tags by data collection intervals. For example, you can put a name plate or static tags where the value rarely changes into one data store, and your process tags into another data store. This can improve query performance.
Historian Data stores are stored archive files that contain data gathered from all data sources during a specific period of time. You can write and read data from the archives available under the data stores. Using data stores, you can store, organize, and manage tags according to the data source and storage requirements.
- Historical Data Store: Tags stored under historical data store will store data as long as disk space is available. Depending on your license, you may be able to create multiple historical data stores. The maximum number of Historical data stores supported depends on the license.
- SCADA Buffer Data Store: Tags stored under the SCADA buffer data store will store data for a specific duration of time based on license.
- System: Stores Historian messages and performance tags. This is only for internal usage within Historian, and you cannot add tags to this data store. You cannot rename or delete the System data store.
- User: Stores the data for the tags. This is a default data store. You can rename and delete a user data store as long as there is another default data store set for tag addition.
- SCADA Buffer: Stores short term tags and data in a SCADA Historian data store.
Moving Tags Between Data Stores
About this task
When you move a tag, only the tag itself is moved; the data already associated with that tag does not automatically move with it. Moving the old data is optional, but if the old data is not moved to the new data store, it cannot be retrieved.
Procedure
What to do next
Before moving any data, best practice is to back up the archive file(s) that contain the old data.
Adding a Data Store
About this task
Procedure
What to do next
Deleting a Data Store
About this task
Procedure
Editing a Data Store
About this task
/ \ * ? < > |