Historian creates the following types of log files:
- The .IHA files: These files contain data about archives. They are created
by the Historian server after data collection begins. By default, these files
are located in the C:\Historian Data\Archives folder.
- The .IHC files: These files contain data about Historian configuration.
They are created by the Historian server. By default, these files are located in
the C:\Historian Data\Archives folder.
There are two
types of .IHC files:
- *CentralConfig.ihc: This is the master
configuration file used by Configuration Manager.
- *config.ihc: This is used by the data archiver
and is generated from *CentralConfig.ihc. This
is to maintain consistency between Historian versions.
- The .LOG files: These files contain logging data (such as events,
warnings, and errors). They are created by the archiver and the collectors. By
default, they are located in the C:\Historian Data\LogFiles
folder.
- The .SHW files: These files contain configuration data. They are created
by the archiver and the collectors. By default, they are located in the
C:\Historian Data\LogFiles folder.