Set a Default System

About this task

If you set a system as default, when you log in to Configuration Hub, this system appears by default. The following conditions apply when you set a system as default:
  • You can have only one default system in Configuration Hub.
  • You cannot delete a default system.

Procedure

  1. Access the system that you want to set as default.
  2. In the upper-right corner of the main section, select , and then select Set Default System.
    The system is set as default, indicated by .