Delete a Historian System

About this task

You can delete a Historian system if you no longer want to manage it using Configuration Hub. You cannot, however, delete a system if it is set as default.

Procedure

  1. Access Configuration Hub.
  2. In the Navigation section, select the Historian system that you want to delete.
  3. In the upper-right corner of the main section, select , and then select Delete.
    A message appears, asking you to confirm that you want to delete the Historian system.
    Note: The Delete button is disabled for a default Historian system.
  4. Select Delete.
    The Historian system is deleted.