Install Collectors Using the Installer
About this task
After you install collectors, the following artefacts will
be available:
This topic describes how to install collectors using a
GUI-based installer. You can also intall them at a command prompt.- Executable files: These files are required to add a collector instance.
- The Remote Collector Management agent: Provides the ability to manage collectors remotely.
Procedure
What to do next
- Ensure that the Windows user that you have specified while installing collectors is added to the iH Security Admins and iH Collector Admins groups.
- Enable trust for a client certificate for Configuration Hub.
- Enable trust for a self-signed certificate on Chrome.
- Import an issuer certificate.
You are now ready to use Configuration Hub. To add and manage collector instances, you can use Configuration Hub or Remote Collector Management. For instructions specific to setting up the iFIX collector and the iFIX Alarms and Events collector, refer to Working with iFIX Collectors.