Changing Alarm Timestamp Check Intervals

About this task

Use the following procedure to speed up, slow down, or disable alarm timestamp checking,

Procedure

  1. From the Start menu, select Run and enter Regedit.
  2. Open the following key folder. HKEY_LOCAL_MACHINE\SOFTWARE\Intellution, Inc.\iHistorian\Services\DataArchiver\
  3. Create a new DWORD called AlarmTimestampCheck and set its value to 1.
    Set AlarmTimestampCheck to 0 to turn off timestamp checking entirely. Set AlarmTimestampCheck to 2 for slower timestamp checking.
  4. Select OK.
  5. Close the Registry Editor.
  6. Restart the Data Archiver for the changes to take effect.