Important: You do not have the latest version of Historian! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the Historian product page. For more information on upgrades, contact your GE Digital sales agent or e-mail GE Digital Sales Support. For the most up-to-date documentation, go here.
Reusing Archive Configuration Files
About this task
You may want to reuse an existing archive configuration file (*.ihc) when a Historian installation uses the same archive configuration as another Historian installation or when renaming a machine and reusing the original .ihc file.
Procedure
Retrieve a copy of the <oldmachinename>_CentralConfig.ihc file from the old machine. By default, this is located at C:\Proficy Historian Data\Archives
On the new machine, select and stop the following services: Historian Client Manager, Historian Configuration Manager, Historian Data Archiver, and Historian Diagnostics Manager.
Stop services using the Services application, which is part of the Windows Administrative Tools.
Copy the <oldmachinename>_CentralConfig.ihc file into the local folder on the new machine where the .ihc files reside.
Look for a file in that folder on the new machine named <newmachinename>_CentralConfig.ihc If there is a file with that name, delete it.
Rename the copied .ihc file on the new machine to <newmachinename>_CentralConfig.ihc.
Run a command prompt with "Run as Administrator".
Go to C:\Program Files\Proficy\Proficy Historian\x64\Server and run the following command: ihConfigManager_x64.exe RenameDHSNode <oldmachinename><newmachinename>