Adding Nested Domain Groups to Historian Security Groups
The following procedure describes, a European domain group user trying to connect to Historian server, installed in India.Europe.US.com Domain Controller.
Procedure
- Create a user EuropeGroupUser1 in Europe.US.com DC.
- Create a group EuropeGroup1.
- Add the EuropGroupUser1 to EuropeGroup1.
- Add the group (i.e. EuropeGroup1) from Europe.US.com to “IH Security Admin” group in India.Europe.US.com DC
- Login to Historian Client using EuropeGroupUser1.
- If a new user gets added to EuropeGroup1 then it gets automatically synced with Historian Security Groups.Note:
- As EuropeGroupUser1 added as a IH Security Admin, user will get full access to Historian Server.
- When there is a change to EuropeGroup1 (Add/Delete/Modify users), it gets automatically synchronized with Historian Security Groups. The synchronization time is configurable using Data Archiver options as shown below:
ihDataArchiver_x64 ihArchiverMultiADSISyncInterval <Number of hours>
Default is “6” hours and user can configure between1 to 120 hours.
US domain group user trying to connect to Historian Server installed in India.Europe.US.com Domain Controller.
- Create a user USGroupUser1 in US.com DC (if not exist).
- Create a group USGroup1.
- Add the USGroupUser1 to USGroup1.
- Add the group (i.e. USGroup1) from US.com to “IH Security Admin” group in India.Europe.US.com DC
- Login to Historian Client using USGroupUser1.
- If a new user gets added to USGroup1 then it gets automatically synced with Historian Security Groups.
Note:- As USGroupUser1 added a IH Readers, user will get data read access to Historian Server
- When there is a change to USGroup1 (Add/Delete/Modify users), it gets automatically synchronized with Historian Security Groups. The synchronization time is configurable using Data Archiver options as shown below:
ihDataArchiver_x64 ihArchiverMultiADSISyncInterval <Number of hours>
Default is “6” hours and user can configure between1 to 120 hours.