COLLECTOR NAME |
The name of the collector instance. If you select the
link in this column, the details of the collector instance
appears. |
COMPRESSION |
The effectiveness of collector compression. If the value
is low, you can increase the compression deadbands to pass
fewer values and thus increase the effect of
compression. |
CONFIGURATION |
The source of the tag configuration for the collector.
Contains one of the following values:
- HISTORIAN: Indicates that
tags are configured using Historian
Administrator.
- OFFLINE: Indicates that tags
are configured using an offline configuration file.
|
MACHINE |
The name of the machine on which the collector is
installed. |
OUT OF ORDER |
The total number of out-of-order samples for the
collector. |
OVERRUNS |
The total number of data events not collected. In normal
operation and under normal conditions, this value should
always be zero. If the value is not zero, which indicates
that data is being lost, you must take steps to reduce peak
load on the system by increasing the collection
interval. |
REDUNDANCY |
Indicates whether collector redundancy is enabled, which
decreases the likelihood of lost data due to soft- ware or
hardware failures. For information, refer to Collector Redundancy. |
REPORT RATE |
The average rate at which the collector is sending data.
This is a general indicator of load on the
collector. |
STATUS |
The status of the collector. Contains one of the
following values:
- Started
- Stopped
- Running
- Paused
|
TAG COUNT |
The number of tags for which the collector collects
data. |
VERSION |
The version number of the collector. |