Recalculate Tag Values Manually
About this task
One instance when you might want to recalculate data would be after the Historian server restores a lost connection. During the period of connection loss, the collector buffers data. When the connection is restored, the buffered data is forwarded to the Historian Server.
When the buffered data arrives, the timestamps are earlier than the most recent calculation
timestamp. Since the timestamp is earlier, polled calculations are not performed again with
the new data unlike the unsolicited calculations. Hence, it is possible that calculations
performed for tags during and after the connection loss might not be entirely accurate.
Therefore, you can recalculate tag data for the time period during and after the connection
loss. The recalculated data will use the most accurate values in calculations.
Note: You can
still use manual recalculation without automatic recalculation by disabling the automatic
recalculation feature. To disable the automatic recalculation, set the Max
Recovery Time to 0 in the Configuration section of the
Collector Maintenance page of the collector.