Mode Editor window Description
The following elements describe the Mode Editor interface.
Number | Component | Description |
---|---|---|
![]() | Sampling Mode |
Sampling modes include the following:
Note: The default mode for the first chart you create uses the Interpolate mode with a sample size of 1000. See your System Administrator to increase the sample size. Please refer to Historian eBooks for an explanation of Sampling Modes.
|
![]() | Sample Increment | The sample increment for all modes, except Calculated, is either: By Size or By Time. When you select By Time, an additional window appears. When you select the Calculated sampling mode, an additional Calculation drop-down menu provides you with a list of the following associated selections:
Note:
Please refer to Historian eBooks for an explanation of Calculation Modes. |
![]() | By Time | This window appears only when you select the Sample Increment. By Time increments appear in a drop-down menu that contains:
|
![]() | Apply Apply to All | Applies the time selections to only the object selected. Applies the time selections to all relevant objects. |