Time Editor window

The Time Editor window allows you to configure the time range for which you want to view data within a chart by entering a start and stop time. For more information on setting time, refer to Configure Time.

Note:
  • The default Start time for the first chart you create is the previous hour (1-hour relative time default).
  • The clock is not active when you leave the Analysis section open and time elapses until you start creating charts. For example, if you open the Analysis section and walk away from your computer for an hour and then create a chart, your chart will be "Stale" as the time period for the fetch is defined by the Start and End time in the editor. This becomes apparent if you also create a Value Card or Current Value Table with the same tag. The values and timestamps will be off by an hour.
Figure: Time Editor window