Tag Attributes Available when Browsing
While some of these attributes are queried on a browse, they are not shown in the browse interface. These attributes are used when adding a tag, but it is not visible to you whether all attributes come from the server or not.
The following table outlines tag attribute availability when browsing.
Attribute | Capability |
---|---|
Tagname
| Yes |
Source Address
| Yes |
Engineering Unit Description
| Yes, varies by the OPC UA Server vendor. |
Data Type
| Yes. |
Hi Engineering Units
| Yes, varies by OPC UA Server vendor. |
Lo Engineering Units
| Yes, varies by OPC UA Server vendor. |
Is Array Tag
| Yes |
Hi Scale
| No |
Lo Scale
| No |