Manual Recalculation
S2S/S2C collector Backfill procedure
With the Recalculate feature you can recalculate all tags for the time period during and after the connection loss. The recalculated tags will use the most accurate values in calculations.
During the period of connection loss, the collector buffers the data. When the connection is restored, the buffered data is forwarded to the Historian Server. When the buffered data arrives, the timestamps show earlier time than the most recent calculation timestamp.
Since the timestamp is earlier, the polled calculations will not execute again with the new data but the unsolicited calculations will re-trigger. Therefore, it is possible that calculations performed for tags during and after the connection loss might be not be entirely accurate.
ihServerToServerCollector.exe RELOADFILENAME=[file location]
RELOADUSERNAME=[Username] <start time> <end time>
Example: C:\Program Files\Proficy\Proficy
Historian\x86\Server>ihServerToServerCollector.exe RELOADFILENAME=c:\taglist.txt
RELOADUSERNAME=\Administrator 1516875659 1516875785
- RELOADFILENAME: This is an optional parameter. File name should be absolute path, this file consists of the tag names, for which Backfill should be performed, each tag should be separated by new line. Any discrepancies in the file/no file exists/parameter not provided leads to Backfill all the tags related to the collector at the current time. After the Backfill, file gets deleted.
- RELOADUSERNAME: This is an optional parameter. This username is used only when destination server is Historian for auditing purpose, and gets ignored when the destination is cloud.
- TIMESTAMP: This parameter accepts Start and end time in seconds in epoch
format for which Backfill should happen. https://www.epochconverter.com/
How Data Recovery works:
- When the recovery logic is executed, the collector will setup subscriptions for all the trigger tags.
- Next, it will recover data. The collector first determines how long it has been since the last write. It compares the current time to data in the registry key
LastCalcRepWriteTime
, which stores the last time data was written to the archive. The collector compares this to the Max Recovery Time that is specified in the user settings and performs a raw data query on the shorter of these two periods. Then it will take the shorter of these two and do a raw data query for all trigger tags. It will then process the returned samples in sequential order based on time. For example, if the collector was shut down for 8 hours, bnut Max Recovery Time was 4 hours, only 4 hours of data would be recovered. - Recovery is performed before real time processing. Once recovery is complete, it will start polling and processing subscriptions in real time. The subscriptions in real time are queued up till the recovery is done.
- Recovery logic will place an end-of-collection marker at the point in time where the collector was shut down. This end-of-collection marker may or may not be there once the recovery is complete. As part of recovery logic, if it calculates a data point exactly at that timestamp where the end-of-collection marker is there, then it will be overwritten with the calculated good data.
- The recovery logic does not write samples to trigger tags or tags that are just in the formula. It is intended to write samples to the calculation tags.
- Messages are added to the log file that indicate when entering and exiting recovery mode.
Examples
- Machine 1:
Runs Data Archiver, iFIX collector (Collector 1), and Calculation collectors.
- Machine 2:
Runs iFIX collector (Collector 2), which collects and sends data to the archiver in Machine 1 (as a Remote Collector).
TagA and TagB are the iFix tags coming from Collector1 and Collector2, respectively. Both of these tags are scanned at a 1-minute poll rate.
Example 1
The following example demonstrates the recovery function for an unsolicited 1-minute interval calculation tag that has a simple current value function.
Create an event based 1-minute interval Calculation Tag (CalcTag1) in Machine 1 consisting of the following calculation: Result=CurrentValue (TagA)
Stop the Calculation collector for 5 minutes and then restart it to trigger data recovery for the 5-minute shutdown period. For the following example, the Calculation collector was stopped at 2002-12-27 17:05:36 and started at 2002-12-27 17:10:48.
Since there is no interruption for the iFIX collector, the raw data query for TagA results the following output:
Raw Data Query for TagA during shutdown period
114) 81 [2002-12-27 17:02:00:00000] Good NonSpecific
115) 72 [2002-12-27 17:03:00:00000] Good NonSpecific
116) 64 [2002-12-27 17:04:00:00000] Good NonSpecific
117) 56 [2002-12-27 17:05:00:00000] Good NonSpecific
118) 39 [2002-12-27 17:06:00:00000] Good NonSpecific
119) 31 [2002-12-27 17:07:00:00000] Good NonSpecific
120) 22 [2002-12-27 17:08:00:00000] Good NonSpecific
121) 14 [2002-12-27 17:09:00:00000] Good NonSpecific
122) 6 [2002-12-27 17:10:00:00000] Good NonSpecific
A raw data query for CalcTag1 during the shutdown period generates the following:
Raw Data Query for CalcTag1 (before recovery)
96) 81 [2002-12-27 17:02:00:00000] Good NonSpecific
97) 72 [2002-12-27 17:03:00:00000] Good NonSpecific
98) 64 [2002-12-27 17:04:00:00000] Good NonSpecific
99) 56 [2002-12-27 17:05:00:00000] Good NonSpecific
100) 0 [2002-12-27 17:05:36:00000] Bad OffLine
Note that an end-of-collection marker is placed at the shutdown point (that is, at 17:05:36) with a bad data quality.
Once the recovery is complete, this is what we see for the recovered CalcTag1. Note that data during the shutdown period is recovered completely. Compare this result set with the one for TagA. Both are the same.
Raw Data Query for CalcTag1 (after recovery)
96) 81 [2002-12-27 17:02:00:00000] Good NonSpecific
97) 72 [2002-12-27 17:03:00:00000] Good NonSpecific
98) 64 [2002-12-27 17:04:00:00000] Good NonSpecific
99) 56 [2002-12-27 17:05:00:00000] Good NonSpecific
100) 0 [2002-12-27 17:05:36:00000] Bad OffLine
101) 39 [2002-12-27 17:06:00:00000] Good NonSpecific
102) 31 [2002-12-27 17:07:00:00000] Good NonSpecific
103) 22 [2002-12-27 17:08:00:00000] Good NonSpecific
104) 14 [2002-12-27 17:09:00:00000] Good NonSpecific
105) 6 [2002-12-27 17:10:00:00000] Good NonSpecific
Also note that the end-of-collection marker is not overwritten by the recovery logic here. If it calculated a data point exactly at the end-of-collection marker, then it would have been overwritten by the calculated good value.
Example 2
The following example demonstrates the recovery function for an unsolicited calculation tag that has multiple triggers.
Create an event based Calculation Tag (CalcTag2) in Machine 1 consisting of the following calculation:
Result=CurrentValue (TagA) + CurrentValue (TagB)
where TagA and TagB are both trigger tags, coming from Collector1 and Collector2 respectively. Set the collection offset of 5 seconds for TagA and 10 seconds for TagB, forcing the calculation to be performed twice per minute.
Stop the Calculation collector for 5 minutes, and then restart it to trigger data recovery for this 5-minutes shutdown period. For the following example, the Calculation collector was stopped at 02/18/2003 12:15:33 and started at 02/18/2003 12:21:53.
Since the iFIX collector was not interrupted, a raw data query for TagA and TagB values generates the following output:
Raw Data Query for TagA during the shutdown period
10) 13 [2003-02-18 12:10:05:00000] Good NonSpecific
11) 12 [2003-02-18 12:11:05:00000] Good NonSpecific
12) 11 [2003-02-18 12:12:05:00000] Good NonSpecific
13) 11 [2003-02-18 12:13:05:00000] Good NonSpecific
14) 10 [2003-02-18 12:14:05:00000] Good NonSpecific
15) 18 [2003-02-18 12:15:05:00000] Good NonSpecific
16) 17 [2003-02-18 12:16:05:00000] Good NonSpecific
17) 16 [2003-02-18 12:17:05:00000] Good NonSpecific
18) 16 [2003-02-18 12:18:05:00000] Good NonSpecific
19) 15 [2003-02-18 12:19:05:00000] Good NonSpecific
20) 14 [2003-02-18 12:20:05:00000] Good NonSpecific
21) 13 [2003-02-18 12:21:05:00000] Good NonSpecific
Raw Data Query for TagB during the shutdown period
10) 35 [2003-02-18 12:10:10:00000] Good NonSpecific
11) 34 [2003-02-18 12:11:10:00000] Good NonSpecific
12) 33 [2003-02-18 12:12:10:00000] Good NonSpecific
13) 32 [2003-02-18 12:13:10:00000] Good NonSpecific
14) 31 [2003-02-18 12:14:10:00000] Good NonSpecific
15) 31 [2003-02-18 12:15:10:00000] Good NonSpecific
16) 39 [2003-02-18 12:16:10:00000] Good NonSpecific
17) 38 [2003-02-18 12:17:10:00000] Good NonSpecific
18) 37 [2003-02-18 12:18:10:00000] Good NonSpecific
19) 36 [2003-02-18 12:19:10:00000] Good NonSpecific
20) 36 [2003-02-18 12:20:10:00000] Good NonSpecific
21) 35 [2003-02-18 12:21:10:00000] Good NonSpecific
A raw data query for CalcTag2 during the shutdown period generates the following:
Raw Data Query for CalcTag2 (before recovery)
12) 50 [2003-02-18 12:09:05:00000] Good NonSpecific
13) 50 [2003-02-18 12:09:10:00000] Good NonSpecific
14) 49 [2003-02-18 12:10:05:00000] Good NonSpecific
15) 48 [2003-02-18 12:10:10:00000] Good NonSpecific
16) 47 [2003-02-18 12:11:05:00000] Good NonSpecific
17) 46 [2003-02-18 12:11:10:00000] Good NonSpecific
18) 45 [2003-02-18 12:12:05:00000] Good NonSpecific
19) 44 [2003-02-18 12:12:10:00000] Good NonSpecific
20) 44 [2003-02-18 12:13:05:00000] Good NonSpecific
21) 43 [2003-02-18 12:13:10:00000] Good NonSpecific
22) 42 [2003-02-18 12:14:05:00000] Good NonSpecific
23) 41 [2003-02-18 12:14:10:00000] Good NonSpecific
24) 49 [2003-02-18 12:15:05:00000] Good NonSpecific
25) 49 [2003-02-18 12:15:10:00000] Good NonSpecific
26) 0 [2003-02-18 12:15:11:00000] Bad OffLine
Once data recovery is complete, this is what we see for the recovered data for CalcTag2. Note that data during the shutdown period is completely recovered:
Raw Data Query for CalcTag2 (after recovery)
12) 50 [2003-02-18 12:09:05:00000] Good NonSpecific
13) 50 [2003-02-18 12:09:10:00000] Good NonSpecific
14) 49 [2003-02-18 12:10:05:00000] Good NonSpecific
15) 48 [2003-02-18 12:10:10:00000] Good NonSpecific
16) 47 [2003-02-18 12:11:05:00000] Good NonSpecific
17) 46 [2003-02-18 12:11:10:00000] Good NonSpecific
18) 45 [2003-02-18 12:12:05:00000] Good NonSpecific
19) 44 [2003-02-18 12:12:10:00000] Good NonSpecific
20) 44 [2003-02-18 12:13:05:00000] Good NonSpecific
21) 43 [2003-02-18 12:13:10:00000] Good NonSpecific
22) 42 [2003-02-18 12:14:05:00000] Good NonSpecific
23) 41 [2003-02-18 12:14:10:00000] Good NonSpecific
24) 49 [2003-02-18 12:15:05:00000] Good NonSpecific
25) 49 [2003-02-18 12:15:10:00000] Good NonSpecific
26) 0 [2003-02-18 12:15:11:00000] Bad OffLine
27) 48 [2003-02-18 12:16:05:00000] Good NonSpecific
28) 56 [2003-02-18 12:16:10:00000] Good NonSpecific
29) 55 [2003-02-18 12:17:05:00000] Good NonSpecific
30) 54 [2003-02-18 12:17:10:00000] Good NonSpecific
31) 54 [2003-02-18 12:18:05:00000] Good NonSpecific
32) 53 [2003-02-18 12:18:10:00000] Good NonSpecific
33) 52 [2003-02-18 12:19:05:00000] Good NonSpecific
34) 51 [2003-02-18 12:19:10:00000] Good NonSpecific
35) 50 [2003-02-18 12:20:05:00000] Good NonSpecific
36) 50 [2003-02-18 12:20:10:00000] Good NonSpecific
37) 49 [2003-02-18 12:21:05:00000] Good NonSpecific
38) 48 [2003-02-18 12:21:10:00000] Good NonSpecific
39) 47 [2003-02-18 12:22:05:00000] Good NonSpecific
40) 46 [2003-02-18 12:22:10:00000] Good NonSpecific
Example 3
The following example demonstrates the recovery function for an unsolicited calculation tag that has multiple triggers, but for which none of the triggers is in the formula.
TagA and TagB are the iFix tags coming from Collector1 and Collector2, respectively. Both tags are scanned at a 1-minute poll rate. This example uses two more iFix tags, TagC and TagD, coming from Collector1.
Create an event-based Calculation Tag (CalcTag3) in Machine 1 consisting of the following calculation:
Result=CurrentValue (TagA) + CurrentValue (TagB)
Make sure that the trigger tags for this calculation tag are TagC and TagD, which are not in the formula. Set the collection offset of 5 seconds for TagC and 10 seconds for TagD, forcing the calculation to be performed twice per minute.
Stop the Calculation collector for 5 minutes, and then restart it to trigger data recovery for this 5-minutes shutdown period. For the following example, the Calculation collector was stopped at 02/18/2003 02:24:37 and started at 02/18/2003 02:31:44.
Since the iFIX collector was not interrupted, a raw data query for TagA and TagB values generates the following output:
Raw Data Query for TagA during shutdown period
56) 13 [2003-02-18 14:21:05:00000] Good NonSpecific
57) 12 [2003-02-18 14:22:05:00000] Good NonSpecific
58) 11 [2003-02-18 14:23:05:00000] Good NonSpecific
59) 11 [2003-02-18 14:24:05:00000] Good NonSpecific
60) 10 [2003-02-18 14:25:05:00000] Good NonSpecific
61) 19 [2003-02-18 14:26:05:00000] Good NonSpecific
62) 18 [2003-02-18 14:27:05:00000] Good NonSpecific
63) 17 [2003-02-18 14:28:05:00000] Good NonSpecific
64) 16 [2003-02-18 14:29:05:00000] Good NonSpecific
65) 16 [2003-02-18 14:30:05:00000] Good NonSpecific
66) 15 [2003-02-18 14:31:05:00000] Good NonSpecific
Raw Data Query for TagB during shutdown period
141) 36 [2003-02-18 14:20:10:00000] Good NonSpecific
142) 36 [2003-02-18 14:21:10:00000] Good NonSpecific
143) 35 [2003-02-18 14:22:10:00000] Good NonSpecific
144) 34 [2003-02-18 14:23:10:00000] Good NonSpecific
145) 33 [2003-02-18 14:24:10:00000] Good NonSpecific
146) 32 [2003-02-18 14:25:10:00000] Good NonSpecific
147) 31 [2003-02-18 14:26:10:00000] Good NonSpecific
148) 31 [2003-02-18 14:27:10:00000] Good NonSpecific
149) 39 [2003-02-18 14:28:10:00000] Good NonSpecific
150) 38 [2003-02-18 14:29:10:00000] Good NonSpecific
151) 37 [2003-02-18 14:30:10:00000] Good NonSpecific
152) 36 [2003-02-18 14:31:10:00000] Good NonSpecific
A raw data query for CalcTag3 during the shutdown period generates the following:
Raw Data Query for CalcTag3 (before recovery)
6) 49 [2003-02-18 14:21:05:00000] Good NonSpecific
7) 49 [2003-02-18 14:21:10:00000] Good NonSpecific
8) 48 [2003-02-18 14:22:05:00000] Good NonSpecific
9) 47 [2003-02-18 14:22:10:00000] Good NonSpecific
10) 46 [2003-02-18 14:23:05:00000] Good NonSpecific
11) 45 [2003-02-18 14:23:10:00000] Good NonSpecific
12) 45 [2003-02-18 14:24:05:00000] Good NonSpecific
13) 44 [2003-02-18 14:24:10:00000] Good NonSpecific
14) 0 [2003-02-18 14:24:11:00000] Bad OffLine
A data query for the recovered CalcTag3 values once data recovery is complete generates the following. Note that data during the shutdown period is completely recovered:
Raw Data Query for CalcTag3 (after recovery)
6) 49 [2003-02-18 14:21:05:00000] Good NonSpecific
7) 49 [2003-02-18 14:21:10:00000] Good NonSpecific
8) 48 [2003-02-18 14:22:05:00000] Good NonSpecific
9) 47 [2003-02-18 14:22:10:00000] Good NonSpecific
10) 46 [2003-02-18 14:23:05:00000] Good NonSpecific
11) 45 [2003-02-18 14:23:10:00000] Good NonSpecific
12) 45 [2003-02-18 14:24:05:00000] Good NonSpecific
13) 44 [2003-02-18 14:24:10:00000] Good NonSpecific
14) 0 [2003-02-18 14:24:11:00000] Bad OffLine
15) 43 [2003-02-18 14:25:05:00000] Good NonSpecific
16) 42 [2003-02-18 14:25:10:00000] Good NonSpecific
17) 51 [2003-02-18 14:26:05:00000] Good NonSpecific
18) 50 [2003-02-18 14:26:10:00000] Good NonSpecific
19) 49 [2003-02-18 14:27:05:00000] Good NonSpecific
20) 49 [2003-02-18 14:27:10:00000] Good NonSpecific
21) 48 [2003-02-18 14:28:05:00000] Good NonSpecific
22) 56 [2003-02-18 14:28:10:00000] Good NonSpecific
23) 55 [2003-02-18 14:29:05:00000] Good NonSpecific
24) 54 [2003-02-18 14:29:10:00000] Good NonSpecific
25) 54 [2003-02-18 14:30:05:00000] Good NonSpecific
26) 53 [2003-02-18 14:30:10:00000] Good NonSpecific
27) 52 [2003-02-18 14:31:05:00000] Good NonSpecific
28) 51 [2003-02-18 14:31:10:00000] Good NonSpecific
29) 49 [2003-02-18 14:32:05:00000] Good NonSpecific
30) 49 [2003-02-18 14:32:10:00000] Good NonSpecific
31) 48 [2003-02-18 14:33:05:00000] Good NonSpecific
32) 47 [2003-02-18 14:33:10:00000] Good NonSpecific