Historian ETL Workflow
To transfer data using Historian ETL, you must perform the following steps.
Step Number | Description | Notes |
---|---|---|
1 | Install Historian ETL. | This step is required. You must install ETL on both the source and destination machines of the data transfer. Note: If you want to upgrade ETL:
|
2 | Extract data from Proficy Historian or PI Server. | This step is required. It involves extracting tag data and compressing it so that it can be transferred to the destination Historian server. |
3 | Transfer the data using BITS, FTP, or any other file-sharing application. | This step is required. It involves setting up the file-sharing application that you want to use and then transferring the data to the machine on which the destination Historian server is installed. |
4 | Load the data into the destination Historian server. | This step is optional. It involves extracting the .zip files transferred by the file-sharing application and then loading the data into the destination Historian server. |
Note: Depending on the use case, you can use these tools independently or together.