About Extracting Data
You can extract data from one of the following sources:
- Proficy Historian: This is performed by the Historian ETL Extract tool as follows:
- Extracts data related to tags into text files, which are named in the following format: YYYYDDMMHHRR_<onsite Historian computer name>.txt. These files are stored in the following folder: <Historian ETL installation location>/Historian ETL Extract/HistFiles.Note: Data related to alarms and events is stored in .lax files. You can choose not to extract data related to alarms and events.
- After a specified number of files are extracted (by default, 6), the files are compressed into a .zip file, which is named in the following format: YYYYDDMMHHRR_<onsite Historian computer name>.zip. These files are stored in the following folder: <Historian ETL installation location>/Historian ETL Extract/ZipFiles.
- Deletes the text files in the <Historian ETL installation location>/Historian ETL Extract/HistFiles folder after they are compressed.
Before you extract data using this tool, you must configure this tool.
- Extracts data related to tags into text files, which are named in the following format: YYYYDDMMHHRR_<onsite Historian computer name>.txt. These files are stored in the following folder: <Historian ETL installation location>/Historian ETL Extract/HistFiles.
- PI Server: This is performed by the Historian ETL PI Extract tool as follows:
- Extracts data related to tags into text files, which are named in the following format: YYYYDDMMHHRR_<onsite Historian computer name>.txt. These files are stored in the following folder: <Historian ETL installation location>/Historian ETL PI Extract/HistFiles.
- After a specified number of files are extracted (by default, 6), the files are compressed into a .zip file, which is named in the following format: YYYYDDMMHHRR_<onsite Historian computer name>.zip. These files are stored in the following folder: <Historian ETL installation location>/Historian ETL PI Extract/ZipFiles.
Note: Encryption is not supported by the Historian ETL PI Extract tool.Before you extract data using this tool, you must configure this tool.