Data Types
The following table lists the data types recommended for use with Historian.
The OPC Classic HDA collector Data Type | Recommended Data Type in Historian |
---|---|
I1- 16 bit signed integer | Single Integer |
I4- 32 bit signed integer | Double Integer |
R8- 64 bit double float | Single Float |
UI2- 16 bit unsigned single integer | Double Float |
UI4- 32 bit unsigned double integer | Unsigned Integer |
UI8- 64 bit unsigned quad integer | Unsigned Double Integer |
I8- 64 bit quad integer | Quad Integer |
BSTR | Variable Sting |
BOOL | Boolean |
I1- 8 bit single integer | Byte |
Note: The OPC Classic HDA
collector requests data from the OPC Classic HDA
server in the native data type. The OPC Classic HDA
collector then converts the received value to a Historian Data Type before sending it to the data archiver.