Configuration of the OPC HDA Collector
Enter the value for the OPC Classic HDA collector-specific field parameters through the OPC HDA Collector Maintenance - Configuration section of Historian Administrator.
Descriptions for collector-specific fields are listed in the following table.
Note: If the following fields are updated, then the collector must be restarted for the
update to take effect.
Field | Description |
---|---|
The OPC Classic HDA server | This field represents the OPC Classic HDA server ProgID to which the collector connects. By default, it points to the OPC Classic HDA server ProgID that was entered at the time of installation. |
Recovery Time (in hours) | This field is used by the collector on start up to get the specified number
of hours of data of the added tags from the OPC Classic HDA
server, and then pushes the
data to Historian.
|