Configuring Recovery Mode
About this task
The default recovery time available is 4 hours. You can disable recovery mode by setting the Maximum Recovery Time to 0 hours.
To configure a maximum recovery time:
Procedure
- Start the Historian Administrator.
- Select the Collectors screen.
- Select OSI PI Collector.
- Click the Configuration tab.
- In the Maximum Recovery Time (hr) field, enter a Maximum Recovery Time, in hours. If this field is left blank, the Maximum Recovery Time will be set to 4 hours.