Renaming Digital States
If digital states are renamed in the PI Collector, the corresponding enumerated sets in Historian are not automatically renamed without a restart of the PI collector. Unused enumerated sets cannot be automatically deleted, because the PI Server does not notify the PI collector about rename activity.
When a digital state is renamed, a new enumerated set is created. There will therefore be two enumerated sets for the same digital set, one of which has the old name and one of which has the new name. The old enumerated set is redundant as it will not get any data if no tag is assigned to it. The tag association is also lost.
- Manually assign the new enumerated set to the applicable tag in Historian. It will then be synchronized to represent the data for the renamed digital state.
- Go to the Historian VB admin and delete the unused enumerated set at the Historian side.
PHsite1.PumpStatus
in Historian is assigned to Tag1
: PI Server | Historian |
---|---|
Site1.PumpStatus | PHSite1.PumpStatus |
ON= 0 | OFF= 0 |
OFF= 1 | ON= 1 |
If the digital state Site1.PumpStatus
is renamed to SiteLodha.PumpStatus
, a new enumerated set PHSiteLodha.PumpStatus
is created at the Historian side.
The old enumerated set on the Historian side PHSite1.PumpStatus
will not show any data, but it will exist redundantly inside Historian.
To address this:
- Manually assign
Tag1
(applicable tag in Historian) toPHSiteLodha.PumpStatus
. - Go to the Historian VB admin and manually delete the old enumerated
PHSite1.Pump Status
.