ihCalculationDependencies Table
The ihCalculationDependencies table contains the calculation and server-to-server tags and their triggers. The following table describes the columns of the ihCalculationDependencies table.
Column Name | Data Type | Description |
---|---|---|
Tagname | VT_BSTR | A calculation or server-to-server tag with unsolicited collection and at least one dependent tag. |
DependentTagname | VT_BSTR | A dependent tagname. If a tag has multiple dependent tags, there are multiple rows in the table for that tagname. |
RowCount | VT_I4 | Indicates the maximum number of rows that can be returned. A value of 0 indicates that there is no limit to the number of rows returned. |
ihCalculationDependencies Examples
Example SQL statements for the ihCalculationDependencies table are outlined in the following examples.
Example 1: Show the Dependencies for a Specific Tag
SELECT * FROM ihcalculationdependencies WHERE tagname = c1
Example 2: Show the Dependencies for a Specific Dependent Tag
SELECT * FROM ihcalculationdependencies
WHERE dependenttagname=brahms.ai1.f_cv