About the Samples
Historian OLE DB Provider includes samples from various applications that demonstrate some possible applications of the provider. Use these reports directly or modify them to fit your requirements. They are provided as examples, and are not the only way of creating reports in the specified clients. The sample reports are located in the subfolders of the Historian\Samples folder.
The following list outlines the applications for which samples are included:
Note: You must specify a server name or enter a login username and password when you connect to the Historian server from these applications. For instance, in ADO you pass the server name, username, and password in the connect string.