Frequently Asked Questions
The following sections outline some of the most frequently asked questions when using the Historian OLE DB Provider. These questions include:
- How Are Historian Calculation Modes and SQL Aggregate Functions Different?
- How Are the ihTrend and ihRawData Tables Different?
- Can I Run Multiple Applications Using the OLE DB Provider?
- Can I Retrieve Data from Multiple Servers?
- What Is a Session?
- How Do the > and >= Operators Work With Timestamps?
- How Do I Throttle Query Results?
- When Should I Use Excel Instead of the Historian Excel Add-In?
- Why Is the Raw Sample at the Start Time Not Returned?
- What Username and Password Are Used if Not Specified in the Connect String?
- What Is an Array Tag?
- What Is a User-Defined Type?
- What Is Not Supported?