Excel Add-In Options

FieldDescription
Internal vs. External ReferencesChoosing Use External References allows your application to reference cells in other worksheets and workbooks in addition to the current one. If you choose Use Internal References instead, you can only access cells in the current worksheet. The default setting is Use External References.
Automatically Update Links to Add- In (Yes/No)Add-In functions are maintained as worksheet links. If users who share worksheets do not have Microsoft Office installed the same way, it is necessary to turn this feature on. When on, this feature automatically re-establishes any formula links that may be broken due to differences among users in Microsoft Office installation. The default setting enables this feature.

The Auto Update feature allows sharing of worksheets. You must, however, install the Excel Add-In in the exact same Microsoft Office Library Path as the other worksheets if you want to use the sharing feature.

When opening a worksheet with links to another worksheet, you may receive a message prompting you to update all linked information in the workbook (Yes) or keep the existing information (No). It is recommended that you select No and keep the existing information. The links will be automatically updated for your worksheet. Save your worksheet after the links have been updated.

Show/Hide Header LabelsThis option lets you display or suppress the column header labels that are automatically placed in the worksheet when entering formulas throughout the Historian dialogs. The default setting is Show Labels.
ColorAllows you to select the header name color from the drop-down list: black, blue, red, green, magenta, cyan, or yellow.
Assign Default ServerThis dialog box shows the current server assignment. You can modify the setting by clicking the Edit button and accessing the Historian Server Managers dialog box. This dialog box allows you to save user connection information, add or connect to a new server, delete a server, and modify the default server.
Adjust Column WidthsThis option lets you automatically adjust the width of columns in your worksheet as formulas are inserted by Historian dialogs. Click Adjust Header Column Width to modify the width of header labels; click Adjust Data Column Width to modify the data column widths to accommodate the data values. Enabling these options usually makes the worksheet much more readable. However, doing so can sometimes make the worksheet calculate too much when building a large report. In such cases, disable the automatic feature and adjust individual columns manually.
Save/Default/CancelThese action buttons let you apply your choices of options. Click Save to apply the settings you entered, click Default to select default settings for all options, and click Cancel to close the dialog box.