Exporting Enumerated Sets
About this task
The Export Enumerated Sets function enables you to display information about enumerated sets in an Excel worksheet. Using this function, you can export sets data from Historian, add and edit the enumerated sets information, and import it back into Historian.
This feature allows you to make changes in bulk and send them to Historian in a simple procedure without using the Histroian Administrator. Before importing or exporting enumerated sets, you should be aware of a convention used with the Historian application. The Server is the reference point for all import and export functions. If you want to move tag information from the Historian Server into your worksheet, you must use the Export Enumerated Sets command.
Conversely, if you want to move data from your worksheet to the server, you must use the Import Enumerated Sets command. If you plan to import set information, it is recommended that you first export a set, to become familiar with the format.