About this task
The Export MultiField Source Address function enables you to display information of the source address of the multifield tags in an Excel worksheet.
Procedure
- Select Administration and then select Export MultiField Source Addresses from the Historian menu.
The Historian Export MultiField Source Addresses dialog box appears.
- Select a server from the drop-down list. If you do not select a server, the Add-In uses the default server.
- In the Filter Criteria section, in the MultiField Tag Mask/MultiField Tag Name field, search for the sets set you want to export.
You can use one of the following options that are available:
- Enter a * or do not enter any criteria. All the types appear.
- Enter a type name or name mask or description and a description mask (*) criteria. All the types matching the criteria appear.
- In the Export Options section, select either the To New Worksheet, To CSV File, or To XML option.
If you select either the CSV or XML option, you must also enter a path and file name for the destination file.
- Click OK to execute the Export UserDefinedtype function. Click Cancel to cancel and close the dialog box.
When the export function finishes, a dialog box appears within a display of the worksheet containing the exported types and the message, Export Succeeded. Click OK to acknowledge the operation and close the dialog box.