Historian Interactive SQL Application
The Historian Interactive SQL application (ihSQL.exe) is a test program that allows you to run a SQL query and display the results of the query in the same window. It is useful if you need to test or verify a query using the Historian OLE DB Provider. The Historian Interactive SQL application requires that you have some SQL knowledge, since there are no wizards or experts. It can open and save SQL queries and can even show multiple windows, each containing a query request to the same server or different servers.
This application is particularly helpful in troubleshooting OLE DB problems from different client tools. If you are having trouble with a SQL query in Visual Basic or Crystal Reports, try it in the Historian Interactive SQL application first.