Installing Historian Data Collectors
About this task
You can install the data collectors using the Historian product DVD. Observe the following guidelines when you install Historian Data Collectors:
- You can install only one each of the iFIX, Machine Edition View, OSI PI, Alarm and Event, File, Calculation, Server-to-Server, or Simulation Collectors on a given computer.
- You can install multiple OPC Collectors on a single computer, one for each OPC Server that is installed on the machine.
- Expect an increased processing load if your data source uses iFIX networking.Note: iFIX networking does not provide buffering for data from a remote iFIX node. It is recommended that you install a data collector on each iFIX SCADA node to collect data from that iFIX node. This is both faster and more robust.
Installing Historian data collectors:
Procedure
What to do next
Installing Collectors with destination on Predix Cloud
- Select Predix Cloud as the destination for the collector to configure bimodal/cloud capable collector.
- The Cloud Information and Configuration screen appears when you select Predix Cloud. All the information provided in this screen will be saved to HISTORIANNODENAME registry for the collector. It is not recommended to manually update this key post install, as certain fields are auto generated during install and cannot be updated once the install is complete. For information about the fields on this screen, refer to Cloud Information and Configuration Fields. See Reconfigure Cloud Information and Configuration for updating the cloud information after the install.
- The Datapoint Attributes screen appears. The use of datapoint attributes is optional. This can be useful in sending additional metadata to the Predix Time Series. Note: If you want to use Datapoint attributes, more information is available on the Predix website, https://www.predix.io/docs - Services > Data Management Services > TimeSeries.If you do not want to set the data point attributes, skip this screen and click Next.
- The Do you want to use an offline configuration? screen appears.
- If you want to install cloud collector using offline configuration, select Offline Configuration. To know more information about Offline Configuration, refer to Offline Configuration for Collectors.
Or
- If you want to install the cloud collector using historian configuration, select Historian Configuration. For this you must provide the machine address where Historian Server or Historian client tools (Historian Administrator) are installed in order to browse and configure tags.
- Click Next and proceed with further installation.
- If you want to install cloud collector using offline configuration, select Offline Configuration. To know more information about Offline Configuration, refer to Offline Configuration for Collectors.
Silent install of Cloud Collectors
For Silent install of Cloud Collectors, see section: Installing a Collector Silently using the Command Line.
Upgrading cloud collector
Upgrading a cloud collector follows the same steps as upgrading the corresponding Historian Data Collector.