About Historian Data Collectors
The Historian Data Collectors General manual is intended for people who install, use, and maintain data collectors in an Historian archiving system. This manual provides descriptive material and specific operating procedures for performing all common tasks.
Many data collectors exist to bring data into the Historian Server, as listed in Supported Windows Versions for Historian Collectors.
Since installation, maintenance, and troubleshooting from a Historian perspective are essentially the same for all collectors other than the File Collector, this chapter summarizes the characteristics of each and highlights their differences. It also provides a detailed description for File Collector, since it differs from the other types of collectors.

Data Collectors use a specific data acquisition interface matched to the data source type, such as iFIX EDA (Easy Data Access) or OPC 1.0 or 2.0 (Object Linking and Embedding for Process Control). For more information, see Supported Acquisition Interfaces. The Simulation Collector generates random numeric and string data. The File Collector reads data from text files.
Collector Name | Is Toolkit-Based? | Consumes a CAL? |
---|---|---|
iFIX Collector | No | No |
iFIX Alarm Collector | No | No |
Server-to-Server Collector | No | Yes |
Server-to-Server Distributor | No | Yes |
OSI PI Collector | No | No |
Calculation Collector | No | Yes |
OPC UA Data Access (DA) Collector | No | No |
Windows Performance Collector | Yes | Yes |
ODBC Collector | Yes | Yes |
OPC UA Collector | Yes | Yes |
OPC HDA Collector | Yes | Yes |
Wonderware Collector | Yes | Yes |
Cygnet Collector | Yes | Yes |
MQTT Collector | Yes | Yes |
OPC Alarms and Events Collector | No | No |
Simulation Collector | No | No |
File Collector | No | No |
- When failover occurs from a primary collector to a secondary collector (or vice versa), there will be some data loss as the collector tries to connect to the source to fetch the data.