Select the Accept check box to accept the license agreement, and select Next.
If needed, change the installation drive, and then select Next.
If needed, change the port number for the NodeJS server to run. This step is required if the default port number is not available.
Select Next.
Select Install.
The Help is installed.
Select Next.
Results
The standalone Help is installed in the following folder:
<installation drive>:\Program
Files\Proficy\Proficy Historian\ProficyDoc. You can access the Help from
any of the Historian applications or by accessing the index.html
file.