Overview of the OPC UA DA Collector
The OPC UA Data Access (DA) collector gathers and collects data from a OPC UA 1.0-compliant OPC UA DA server (such as CIMPLICITY). The collector automatically determines the capability of the OPC UA DA server to which it is connected, and supports the appropriate features based on this information.
- You can browse the source for tags and their attributes on an OPC server that supports browsing.
- Both the polled and unsolicited data collection are supported; when changes
to the OPC source tags are detected, they are sent to the Historian server.
Unsolicited data collection is supported for OPC 2.0 only. The minimum poll
interval is 100ms. The collector duplicates raw samples from the OPC server
into the Historian data archive.
For unsolicited data collection, if collector compression is disabled, all new values produce an exception. And, the deadband percentage is determined by the collector deadband percent. You can only configure the collector deadband percent by enabling compression.
- The supported timestamp resolution is 1ms.
- Floating point, integer, binary, and string data are supported.
- Python expression tags are supported.
- Device timestamps are accepted.
OPC UA DA Collector Data Type | Recommended Data Type in Historian |
---|---|
OpcUaType_Null |
ihTKVariableString |
OpcUaType_Boolean |
ihTKBool |
OpcUaType_SByte |
ihTKByte |
OpcUaType_Byte |
ihTKByte |
OpcUaType_Int16 |
ihTKInteger |
OpcUaType_UInt16 |
ihTKUInt16 |
OpcUaType_Int32 |
ihTKDoubleInteger |
OpcUaType_UInt32 |
ihTKUInt32 |
OpcUaType_Int64 |
ihTKInt64 |
OpcUaType_UInt64 |
ihTKUInt64 |
OpcUaType_Float |
ihTKFloat
|
OpcUaType_Double |
ihTKDoubleFloat |
OpcUaType_DateTime |
ihTKVariableString |
OpcUaType_Guid
|
ihTKDataTypeUndefined |
OpcUaType_StatusCode
|
ihTKDataTypeUndefined |
OpcUaType_String |
ihTKVariableString |
OpcUaType_ByteString |
ihTKDataTypeUndefined |
OpcUaType_XmlElement |
ihTKDataTypeUndefined
|
OpcUaType_NodeId |
ihTKDataTypeUndefined |
OpcUaType_ExpandedNodeID |
ihTKDataTypeUndefined
|
OpcUaType_DiagnosticInfo |
ihTKDataTypeUndefined
|
OpcUaType_QualifiedName |
ihTKDataTypeUndefined
|
OpcUaType_LocalizedText |
ihTKDataTypeUndefined
|
OpcUaType_ExtensionObject |
ihTKDataTypeUndefined
|
OpcUaType_DataValue |
ihTKDataTypeUndefined
|
- Tagname
- Source Address
- Engineering Unit Description
- Data Type
- Hi Engineering Units
- Lo Engineering Units
- Is Array Tag