To host a Proficy Authentication service, you can use the same machine on which Web-based Clients are installed or a different one. This topic describes how to connect to a Proficy Authentication
service that is set up on a machine different from the one on which you have installed
Web-based Clients.
Procedure
Access the Web Admin console.
Select Not Secure, and then select Certificate.
Select the root CA certificate in the Certificate Path
section.
The Certificate Export Wizard window
appears.
Select the Base-64 encoded X.509 (.CER) format.
Install the certificate in Trusted Root Certification Authorities store.
Rename the certificate file from .cer to .pem.
Access Certificate Management Tool.
Access the External Trust section and import the renamed certificate.
Select No when prompted to restart GeOphubMasterStarter.