Jump to main content
×
Learn more about what Proficy Historian can do for you. Click here for more information on Historian solutions and features.
Get Ready for Proficy 2024! Click here to read about our Proficy 2024 offerings.
Stop a Collector
About this task When you stop a collector, the collector stops collecting
data, and it is disconnected from the destination. If, however, you want the collector
to remain connected to the destination, you can instead pause data collection .
Procedure
Access Configuration Hub .
In the NAVIGATION section, under the Configuration Hub
plugin for Historian, select Collectors .
A list of collectors appears.
Tip: You can filter the
collectors by the system name.
Right-click the collector instance that you want to stop (or select ), and then select
Stop .
The Stop: <collector name> window appears. The
COLLECTOR MACHINE and CURRENT RUNNING
MODE fields are populated and disabled.
If the collector is running in the command-line mode, enter values in the
USERNAME and PASSWORD
fields.
Select Stop .
The collector is stopped, and the data collection is paused. The status
of the collector in the Collectors section changes to
Stopped.