Jump to main content
×
Learn more about what Proficy Historian can do for you. Click here for more information on Historian solutions and features.
Get Ready for Proficy 2024! Click here to read about our Proficy 2024 offerings.
Restart a Collector
About this task
You can restart a collector to stop and start it again.
You can restart a collector only if it is running.
Procedure
-
Access Configuration Hub.
-
In the NAVIGATION section, under the Configuration Hub
plugin for Historian, select Collectors.
A list of collectors appears.
Tip: You can filter the
collectors by the system name.

-
Right-click the collector instance that you want to restart (or select
), and then select
Restart.
The Restart: <collector name> window appears.
The COLLECTOR MACHINE and CURRENT RUNNING
MODE fields are populated and disabled.
-
If the collector is running in the command-line mode, enter values in the
USERNAME and PASSWORD
fields.
-
Select Restart.
The collector is restarted, and the data collection is
resumed.