Create an Object Type
About this task
This topic describes how to create an object type. You can also copy one.
Procedure
- Access Configuration Hub.
-
In the NAVIGATION section, under the Configuration Hub
plugin for Historian, select Model. Alternatively, you
can select Systems, and then in the row containing the
system in which you want to create a model, select
, and then select Browse Model.
The Model section appears. -
In the upper-right corner of the section, select
.
The New Object Type window appears. -
Enter values as described in the following table.
Field Description NAME Enter a name for the object type. A value is required and must be unique. The value that you enter:- Must begin with a letter or a number.
- Can contain up to 256 characters.
- Can include any of the following special characters: /!|#{}%$-_
- Must not include a space or any of the following characters: ~`+^:;.,?"*={}@
DESCRIPTION Enter a description for the object type. -
Select Create.
The object type is created.
-
In the main section, under Object Types, right-click the
object type that you have created (or select
), and then select Edit.
The <object type name> section appears. The OBJECT TYPE TEMPLATE field contains the default template. -
To add variables to the default template:
-
To create a custom template:
The custom template is created, along with the variables. You can add more variables, and include/exclude existing variables later too.
-
In the upper-left corner of the page, select Save.The object type, along with the default template, custom templates, and variables, is created.