Table Properties for an ODBC Data Source

This topic provides a list of table properties that you can define for each tag that you want to extract from an ODBC data source.
Column Name Data Type Description
TableName String Enter the name of the table. A value is required and must match the name of a table you specify in the list of tags.
TagNameColumn String Enter the name of the tag whose data you want to extract from the table. A value is required and must match the name of a tag you specify in the list of tags.
TimestampColumn String Enter the name of the column in the database table from which you want to extract the timestamp values.
ValueColumn String Enter the name of the column in the database table from which you want to extract the tag values.
QualityColumn String Enter the name of the column in the database table from which you want to extract the quality values.
ihOPCBad String Enter the values or range of values whose quality must be considered bad. For example, if a tag value is considered bad when the value is between 0 and 50, enter <ihOPCBad>0-50</ihOPCBad>. You can also enter words and values separated by commas (for example, <ihOPCBad>bad, uneven</ihOPCBad>).

A value is required.

ihOPCGood String Enter the values or range of values whose quality must be considered good. For example, if a tag value is considered good when the value is between 51 and 100, enter <ihOPCGood>51-100</ihOPCGood>. You can also enter words and values separated by commas (for example, <ihOPCGood>good, better, excellent</ihOPCGood>).

A value is required.

ihOPCUncertain String Enter the values or range of values whose quality must be considered uncertain. For example, if a tag value is considered uncertain when the value is 101 or 102, enter <ihOPCUncertain>101,102</ihOPCUncertain>. You can also enter a range of values.
ihOPCNA String Enter the values or range of values whose quality must be considered not applicable. For example, if a tag value is considered not applicable when the value is 103, 104, or 105, enter <ihOPCNA>103,104,105</ihOPCNA>. You can also enter a range of values.
Condition String Enter the condition that you want to use to filter data. For example, if you enter Historian = 1, you can use this condition in a WHERE clause when querying data.