Overview of the Historian ETL Tools
Transferring data from one Historian server to another is typically performed by Proficy Historian collectors. These collectors provide a connected streaming data transfer mechanism (except the Calculation and File collectors). In a system where a steady network connection is not possible or not cost-effective, a periodic file-oriented data transfer is preferred. The Historian Extract, Transform, and Load (ETL) tools consist of a comprehensive set of file-oriented data extraction, transfer, and loading tools.
- Data transfer from any of the following sources:
- An eDNA server
- An ODBC data source
- Proficy Historian
- PI Historian
- Data transfer via radio or low bandwidth cellular connection
- Data transfer where there is no connectivity (read and write using portable media)
- Data transfer for periodic connectivity applications (for example, ships can transfer data when they arrive at a port)
- Data migration from OSI PI Server to Proficy Historian
- Data extraction to import into other applications
- Data import from other applications
- Extract: Using this tool, you can extract time series data from an eDNA server, an ODBC data source, Proficy Historian or PI Server. For Proficy Historian, you can also extract alarms and events data, perform scaling and absolute deadband compression.
- Transform: Using this tool, you can transfer data from an onsite Historian server or an ODBC data source to the destination Historian server using a file-sharing application such as FTP, BITS, and so on.
- Load: Using this tool, you can load data into Proficy Historian. This tool monitors a file directory, unzips the files, and processes them.
- The ETL tools do not support array data.