Supported Attributes
The following table provides a list of the attributes supported by the OPC Classic HDA collector.
Historian Property Type | OPC Classic HDA collector Attributes | Data Type | Description |
---|---|---|---|
Data Type | OPCHDA_ DATA_TYPE | Int16 | The data type for the item. For information, refer to Supported Data Types. |
TagDescription | OPCHDA_ DESCRIPTION | String | The description of the item. |
Engineering Units | OPCHDA_ ENG_UNITS | String | The units for the item (for example, kg/sec). |
Archiving | OPCHDA_ ARCHIVING | Boolean | Indicates whether Historian stores data for this item. The following values are valid:
|
ItemID | OPCHDA_ ITEMID | String | The Historian tag name. This is used to allow filtering in
CreateBrowsemethod . |