OPC Classic HDA Aggregates
In the OPC Classic HDA server, an aggregate is a function that is used to process raw data from an OPC Classic HDA server over a given range of time divided into discrete intervals. These aggregates can be further used to for various purposes, such as visualizing the trends in the data.
The standard aggregates supported are:
- Minimum
- Maximum
- Average
- Nearest
- Before
- After
- GE Interpolative
Consider the following as a Historian Source for the Minimum, Maximum and Average Aggregates:
Timestamp | Value | Quality | Notes |
---|---|---|---|
Jan-01-2002 12:00:00 | 0 | No Data | First archive entry Point Created |
Jan-01-2002 12:00:10 | 10 | Raw, Good | |
Jan-01-2002 12:00:20 | 20 | Raw, Good | |
Jan-01-2002 12:00:30 | 30 | Raw, Good | |
Jan-01-2002 12:00:40 | 40 | Raw, Bad | Scan failed, Bad data entered |
Jan-01-2002 12:00:50 | 50 | Raw, Good | |
Jan-01-2002 12:01:00 | 60 | Raw, Good | |
Jan-01-2002 12:01:10 | 70 | Raw, Bad | Value is flagged as questionable |
Jan-01-2002 12:01:20 | 80 | Raw, Good | |
Jan-01-2002 12:01:30 | 90 | Raw, Good | |
NULL | No Data | No more entries, awaiting next scan. |
Timestamp | Value | Quality | Notes |
Feb-28-2002 12:01:30 | 987 | Raw, Bad | |
Mar-01-2002 12:01:30 | 98765 | Raw, Good | |
Mar-02-2002 12:01:30 | 9876 | Raw, Bad | |
Jan-01-2002 12:00:00 | 0 | No Data | First archive entry Point Created |
Jan-01-2002 12:00:10 | 10 | Raw, Good | |
Jan-01-2002 12:00:20 | 20 | Raw, Good | |
Jan-01-2002 12:00:30 | 30 | Raw, Good | |
Jan-01-2002 12:00:40 | 40 | Raw, Bad | Scan failed, Bad data entered |
Jan-01-2002 12:00:50 | 50 | Raw, Good | |
Jan-01-2002 12:01:00 | 60 | Raw, Good | |
Jan-01-2002 12:01:10 | 70 | Raw, Bad | Value is flagged as questionable |
Jan-01-2002 12:01:20 | 80 | Raw, Good | |
Jan-01-2002 12:01:30 | 90 | Raw, Good |