After Aggregate
When the After aggregate function is called with a timestamp (Start time), next valid value after ‘Start time’ will be fetched. This search will happen between Start time and (Start time + MaxDurationSec).
The call for the aggregation is initiated by the source client. The custom aggregations do not require any interval value. The default value for MaxDurationSec is 100 days.
Note:
To change the value of MaxDurationSec navigate to HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Intellution, Inc.\iHistorian\HDAServer
. Create a string value with name MaxDurationSec and provide the value in seconds.
Start: Feb-01-2002 12:00:10 End: NA Interval: NA
Timestamp | Value | Quality |
Mar-01-2002 12:01:30 | 98765 | Raw, Good |