Have You Seen Historian Lately?Click here to check out all the new features in the latest version.
Supercharge your GE solution! Download a free trial of Proficy Operations Hub, CSense analytics, and more. Learn more about the Proficy 2022 releases, by signing up for one of our upcoming events.
Reading and writing to deep trees with large time ranges can be very inefficient. Create a MaxIndexRecursionDepth registry key to configure the depth at which the archiver will warn about deep data trees.
Procedure
From the Start menu, select Run, and then enter Regedit.
Open the following key folder: HKEY_LOCAL_MACHINE\SOFTWARE\Intellution, Inc.\iHistorian\Services\DataArchiver
Create a value as DWORD called MaxIndexRecursionDepth.
Set MaxIndexRecursionDepth to a number higher or lower than the default value of 900.
To get more warning messages, set a smaller number if you have an archive which is 10 to 100 deep.
Select OK.
Close the Registry Editor.
Restart the archiver for the changes to take effect.