Have You Seen Historian Lately?Click here to check out all the new features in the latest version.
Supercharge your GE solution! Download a free trial of Proficy Operations Hub, CSense analytics, and more. Learn more about the Proficy 2022 releases, by signing up for one of our upcoming events.
Ensure that you have a mechanism to generate future data that you want to store in Historian.
About this task
By default, Historian stores up to 1200 seconds of future data. However, if you enable storage of future data, you can store data up to the following timestamp: 03:14:07 on Tuesday, 19 January, 2038. This topic describes how to enable storage of future data.
Procedure
For each data store for which you want to store future data:
Enable the ihArchiverAllowFutureDataWrites option.
This is to avoid receiving an outside-active-hours error. It happens if you attempt to store data when the current archive file is set to read-only.
Tip: You can perform this step using Command Line.
For each collector that sends data to the data store, set the Time Assigned By property to Source.
Note: You can perform this step only for the OPC Data Access, OPCUA Data Access, and OPC Classic HDA
collectors.
Results
Future data is now stored in Historian. You can retrieve the data using any of the available options such as Historian Administrator, Rest APIs, Excel Add-In, and the Historian Interactive SQL application (ihsql.exe).