Have You Seen Historian Lately?Click here to check out all the new features in the latest version.
Supercharge your GE solution! Download a free trial of Proficy Operations Hub, CSense analytics, and more. Learn more about the Proficy 2022 releases, by signing up for one of our upcoming events.
Ensure that you have a mechanism to generate future data that you want to store in Historian.
About this task
By default, Historian stores up to 1200 seconds of future data. However, if you enable storage of future data, you can store data up to the following timestamp: 03:14:07 on Tuesday, 19 January, 2038. This topic describes how to enable storage of future data using Command Line. You can perform this task for any data store other than the default USER data store.
Procedure
Stop the Historian DataArchiver service.
Open Command Prompt with elevated privileges or administrator privileges.
Navigate to the folder in which the ihDataArchiver_x64.exe
file is located. By default, it is C:\Program Files\Proficy\Proficy
Historian\x64\Server.
Run the following command: ihDataArchiver_x64 OPTION.<data store
name> ihArchiverAllowFutureDataWrites 1
Run the following command: ihDataArchiver_x64 OPTION.<data store
name> ihArchiveActiveHours <number of active hours>