Have You Seen Historian Lately?Click here to check out all the new features in the latest version.
Supercharge your GE solution! Download a free trial of Proficy Operations Hub, CSense analytics, and more. Learn more about the Proficy 2022 releases, by signing up for one of our upcoming events.
This topic describes how to enable offline archive creation. This is to avoid receiving an outside-active-hours error. It happens if you attempt to store data when the current archive file is set to read-only.
Procedure
Stop the Historian DataArchiver service.
Open Command Prompt with elevated privileges or administrator privileges.
Navigate to the folder in which the ihDataArchiver_x64.exe
file is located. By default, it is C:\Program Files\Proficy\Proficy
Historian\x64\Server.
To enable the ihArchiveCreateOfflineArchive option for a data
store, run the following command: ihDataArchiver_x64 OPTION.<data
store name> ihArchiveCreateOfflineArchive 1
To enable the ihArchiverAllowFutureDataWrites option:
Run the following command: ihDataArchiver_x64 OPTION.<data
store name> ihArchiverAllowFutureDataWrites 1
Set the Read only After(Hrs) property ::::
[specify value in number of hours)]ihDataArchiver_x64
OPTION.<data store name> ihArchiveActiveHours <number of
active hours>.