Have You Seen Historian Lately?Click here to check out all the new features in the latest version.
Supercharge your GE solution! Download a free trial of Proficy Operations Hub, CSense analytics, and more. Learn more about the Proficy 2022 releases, by signing up for one of our upcoming events.
This topic describes how to delete a custom template. You cannot delete a template
that is in use (that is, an object instance has been created for the object type). And,
you cannot delete the default template in an object type.
In the NAVIGATION section, select
Model. Alternatively, you can select
Systems, and then in the row containing the system in
which you want to create a model, select , and then select Browse
Model.
The Model section appears.
In the main section, under Object Types, right-click the
object type from which you want to delete a template (or select ), and then select
Edit.
The <object type name> section appears. The
OBJECT TYPE TEMPLATE field contains the default
template.
In the OBJECT TYPE TEMAPLTE field, select the template
that you want to delete.
Next to the OBJECT TYPE TEMPLATE field, select, and then select
Delete.
A message appears, asking you to confirm that you want to delete the
template.
Select Yes.
The template is deleted.
In the upper-left corner of the page, select Save.