Have You Seen Historian Lately?Click here to check out all the new features in the latest version.
Supercharge your GE solution! Download a free trial of Proficy Operations Hub, CSense analytics, and more. Learn more about the Proficy 2022 releases, by signing up for one of our upcoming events.
In the NAVIGATION section, select
Model. Alternatively, you can select
Systems, and then in the row containing the system in
which you want to create a model, select , and then select Browse
Model.
The Model section appears.
Under Object Instances, right-click the object instance
that you want to delete (or select ), and then select
Delete.
A message appears, asking you to confirm that you want to delete the
object instance. If there are direct variables in the object type, you can also
choose to delete the tags associated with these variables (along with their
data).
Select Yes.
The object instance is deleted, along with the underlying variables and
templates.