Upgrading Edge OS Via Edge Manager
Procedure
- Login to Edge Manager.
- Navigate to .
- From the Action drop-down menu, select Upload. The Upload dialog will appear.
- Within the dialog, enter the following:
- Name (required): Value must begin with alphanumeric, can contain alphanumeric, hyphens, and underscores. Spaces and periods are not allowed.
- Version (required): Value must be in the format: <major>.<minor>.<bugfix> with 18 digits maximum for each number (e.g., '1.10.2').
- Type: Select Operating System.
- Platform: Select Predix Edge.
- File: Click Choose File to navigate to where your software upgrade file was saved.
- Vendor, Description and Notes are optional fields, however it is recommended to enter something helpful in Description and/or Notes.
- Click Upload.
- Navigate to .
- Select the device(s) for which you want to perform the upgrade.
- From the Device Operations drop-down menu, select Deploy Software.
- The Select Software dialog will appear. Select the uploaded upgrade file and click Next.
- In the Schedule Deployment dialog, select the date and time for deployment to the device.Note:You can set the time zone timestamp formatting (UTC or local) in the Settings page.The Deployment Status dialog appears.
- Click Close.
- To monitor the status of the upgrade, click the device the upgrade is being performed on; select Software from the menu, the upgrade procedure will be listed in the table.