Rebooting the Predix Edge OS VM

From the Predix Edge Technician Console, you can reboot the VM on which Predix Edge OS is running.

Procedure

  1. From the Device Status page, click Device Setup in the left navigation pane.
  2. Click the Utilities tab.
  3. Click Reboot.
    Predix Edge OS and the VM on which it is running restart. This also restarts the Predix Edge Technician Console, which means you will need to sign in again.